I can't find an example with lpuart rx callback

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I can't find an example with lpuart rx callback

1,346件の閲覧回数
gnichimohamed
Contributor III

Hello, i need help

 

Can anyone point me to an example using lpuart with rx callback function for KL03Z

 

Please help

ラベル(1)
0 件の賞賛
返信
1 返信

920件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Gnichi,

Do you use the KSDK ? If yes, there is a  UART callback demo, you can refer to.

it write under KSDK1.2 , while KSDK1.3  demo is the same method to configure,

and pay attention to the bug which Ningning Yu mentioned .

https://community.freescale.com/thread/359899#538622

Hope it can helps

Alice

0 件の賞賛
返信