How does the KDS_1.1.0 KSDK_1.0.0 support ADC Channel Mux?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How does the KDS_1.1.0 KSDK_1.0.0 support ADC Channel Mux?

ソリューションへジャンプ
2,024件の閲覧回数
davestarkey
Contributor II

I am developing a  K64F product using KDS_1.1.0and KSDK_1.0.0. I have gotten GPIO, Timer, USB and UART functions to work from the SDK. I need to use the ADC Channel Mux.

Does the SDK support it?

if not will PE work with the SDK?

When will PE be compatible with the SDK?

 

The Kinetis SDK API Reference Manual.pdf - 3.2.0.24 (page 27) says:

• Channel Mux - Multiple channels share the converter in each ADC instance because of the time

division multiplexing. However, the converter can only handle one channel at a time. To get the

value of an indicated channel, the channel mux should be set to the connection between an indicated

pad and the converter’s input. The conversion value during this period is for the channel only. The

API functions configure the channel.

 

I don't see how this explains how to set up the channel mux. I don't see any functions in the API to do it.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,878件の閲覧回数
davestarkey
Contributor II

Ok, :smileyhappy:

So in depth reading of the SDK and going thru the PE code it is clear that the Mux sequencing functions

actually happened in interrupt service routines. PE is just great I have been using Freescale parts

and I have configured at least 7 designs using Kinetis and DSC parts. With PE this stuff just

works...

That being said the ADC still does not work but at least callback the interrupt is happening.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,879件の閲覧回数
davestarkey
Contributor II

Ok, :smileyhappy:

So in depth reading of the SDK and going thru the PE code it is clear that the Mux sequencing functions

actually happened in interrupt service routines. PE is just great I have been using Freescale parts

and I have configured at least 7 designs using Kinetis and DSC parts. With PE this stuff just

works...

That being said the ADC still does not work but at least callback the interrupt is happening.

0 件の賞賛
返信