Yes, youre right!
I tested it, and used this examples.
I found that I cant use functions: `mbedtls_net_init()' `mbedtls_net_connect()' `mbedtls_net_recv()' etc from net_sockets.h.
I try build my client by using server example for k64f.
Maybe u have any simple example of mbedTLS client working on k64f? (only writting and/or reading messages)
Now my main():
int main(void)
{
struct netif fsl_netif0;
int ret;
ip4_addr_t fsl_netif0_ipaddr, fsl_netif0_netmask, fsl_netif0_gw;
ethernetif_config_t fsl_enet_config0 = {
.phyAddress = EXAMPLE_PHY_ADDRESS,
.clockName = EXAMPLE_CLOCK_NAME,
.macAddress = configMAC_ADDR,
};
SYSMPU_Type *base = SYSMPU;
BOARD_InitPins();
BOARD_BootClockRUN();
BOARD_InitDebugConsole();
base->CESR &= ~SYSMPU_CESR_VLD_MASK;
time_init();
#if FSL_FEATURE_SOC_LTC_COUNT
LTC_Init(LTC0);
#endif
{
#if defined(FSL_FEATURE_SOC_TRNG_COUNT) && (FSL_FEATURE_SOC_TRNG_COUNT > 0)
trng_config_t trngConfig;
TRNG_GetDefaultConfig(&trngConfig);
trngConfig.sampleMode = kTRNG_SampleModeVonNeumann;
TRNG_Init(TRNG0, &trngConfig);
#elif defined(FSL_FEATURE_SOC_RNG_COUNT) && (FSL_FEATURE_SOC_RNG_COUNT > 0)
RNGA_Init(RNG);
RNGA_Seed(RNG, SIM->UIDL);
#endif
}
IP4_ADDR(&fsl_netif0_ipaddr, configIP_ADDR0, configIP_ADDR1, configIP_ADDR2, configIP_ADDR3);
IP4_ADDR(&fsl_netif0_netmask, configNET_MASK0, configNET_MASK1, configNET_MASK2, configNET_MASK3);
IP4_ADDR(&fsl_netif0_gw, configGW_ADDR0, configGW_ADDR1, configGW_ADDR2, configGW_ADDR3);
lwip_init();
netif_add(&fsl_netif0, &fsl_netif0_ipaddr, &fsl_netif0_netmask, &fsl_netif0_gw,
&fsl_enet_config0, ethernetif0_init, ethernet_input);
netif_set_default(&fsl_netif0);
netif_set_up(&fsl_netif0);
mbedtls_ssl_init(&ssl);
mbedtls_ssl_config_init(&conf);
#if defined(MBEDTLS_SSL_CACHE_C)
mbedtls_ssl_cache_init(&cache);
#endif
mbedtls_x509_crt_init(&srvcert);
mbedtls_pk_init(&pkey);
mbedtls_entropy_init(&entropy);
mbedtls_ctr_drbg_init(&ctr_drbg);
#if defined(MBEDTLS_DEBUG_C)
mbedtls_debug_set_threshold(DEBUG_LEVEL);
#endif
ret = mbedtls_x509_crt_parse(&srvcert, (const unsigned char *)mbedtls_test_srv_crt, mbedtls_test_srv_crt_len);
if (ret != 0)
{
PRINTF(" failed\r\n ! mbedtls_x509_crt_parse returned %d\r\n\r\n", ret);
goto exit;
}
ret = mbedtls_x509_crt_parse(&srvcert, (const unsigned char *)mbedtls_test_cas_pem, mbedtls_test_cas_pem_len);
if (ret != 0)
{
PRINTF(" failed\r\n ! mbedtls_x509_crt_parse returned %d\r\n\r\n", ret);
goto exit;
}
ret = mbedtls_pk_parse_key(&pkey, (const unsigned char *)mbedtls_test_srv_key, mbedtls_test_srv_key_len, NULL, 0);
if (ret != 0)
{
PRINTF(" failed\r\n ! mbedtls_pk_parse_key returned %d\r\n\r\n", ret);
goto exit;
}
if ((ret = mbedtls_ctr_drbg_seed(&ctr_drbg, mbedtls_entropy_func, &entropy, (const unsigned char *)pers,
strlen(pers))) != 0)
{
PRINTF(" failed\r\n ! mbedtls_ctr_drbg_seed returned %d\r\n", ret);
goto exit;
}
if ((ret = mbedtls_ssl_config_defaults(&conf, MBEDTLS_SSL_IS_CLIENT, MBEDTLS_SSL_TRANSPORT_STREAM,
MBEDTLS_SSL_PRESET_DEFAULT)) != 0)
{
PRINTF(" failed\r\n ! mbedtls_ssl_config_defaults returned %d\r\n\r\n", ret);
goto exit;
}
mbedtls_ssl_conf_rng(&conf, mbedtls_ctr_drbg_random, &ctr_drbg);
mbedtls_ssl_conf_dbg(&conf, my_debug, NULL);
#if defined(MBEDTLS_SSL_CACHE_C)
mbedtls_ssl_conf_session_cache(&conf, &cache, mbedtls_ssl_cache_get, mbedtls_ssl_cache_set);
#endif
mbedtls_ssl_conf_ca_chain(&conf, srvcert.next, NULL);
if ((ret = mbedtls_ssl_conf_own_cert(&conf, &srvcert, &pkey)) != 0)
{
PRINTF(" failed\r\n ! mbedtls_ssl_conf_own_cert returned %d\r\n\r\n", ret);
goto exit;
}
if ((ret = mbedtls_ssl_setup(&ssl, &conf)) != 0)
{
PRINTF(" failed\r\n ! mbedtls_ssl_setup returned %d\r\n\r\n", ret);
goto exit;
}
printf("starting client https\n\r");
err_t connected;
while (1)
{
connected = httpd_mbedtls_client_init(&ssl);
while(connected == ERR_OK)
{
ethernetif_input(&fsl_netif0);
sys_check_timeouts();
}
if(connected != ERR_OK)
{
printf("not connected\n\r");
}
}
exit:
return -1;
}
function httpd_mbedtls_client_init();
err_t httpd_mbedtls_client_init(mbedtls_ssl_context *ssl)
{
struct tcp_pcb *pcb;
ip4_addr_t dest;
err_t err;
IP4_ADDR(&dest, 192, 168, 0, 102);
pcb = tcp_new();
err = tcp_connect(pcb, &dest, HTTPS_CLIENT_PORT, client_connected);
if (err != ERR_OK)
{
printf("\n tcp_connect(): Errors on return value, returned value is %d\n", err);
}
else
{
printf("\n tcp_connect(): connected\n\r");
}
ssl_p = ssl;
return err;
}
And function client_connected:
static err_t client_connected(void *arg, struct tcp_pcb *pcb, err_t err)
{
printf("client connected function \n\r");
unsigned char bufor[1024];
int ret = 1, len;
LWIP_UNUSED_ARG(arg);
if (err != ERR_OK)
{
printf("\nclient_connected(): err argument not set to ERR_OK, but is value is %d\n", err);
}
else
{
if( ( ret = mbedtls_ssl_set_hostname( &ssl, "Bony_x" ) ) != 0 )
{
printf( " failed\n ! mbedtls_ssl_set_hostname returned %d\n\n", ret );
return -1;
}
mbedtls_ssl_set_bio(&ssl, &ssl_p, mbedtls_net_send, mbedtls_net_recv, NULL);
printf("Starting the TLS handshake...\n");
do {
ret = mbedtls_ssl_handshake(&ssl);
} while(ret != 0 &&
(ret == MBEDTLS_ERR_SSL_WANT_READ ||
ret == MBEDTLS_ERR_SSL_WANT_WRITE));
if (ret < 0) {
printf("mbedtls_ssl_handshake() returned -0x%04X\n", -ret);
return ret;
}
printf("Successfully completed the TLS handshake\n");
}
return err;
}
Now I should to make functions "mbedtls_net_send" and "mbedtls_net_recv".
Looks ok?
Regards,
Bony