HAL vs peripheral driver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HAL vs peripheral driver

12,136 次查看
gibson486
Contributor I

Hopefully this is not a dumb question, but what is the difference between the HAL and peripheral driver?

标签 (1)
0 项奖励
回复
1 回复

6,914 次查看
DavidS
NXP Employee
NXP Employee

Hi Andrew,

If you download and install the KSDK_1.3 to work with the KDS_3.0 (or other IDE's) you can open and read the following:

C:\Freescale\KSDK_1.3.0\doc\Kinetis SDK v.1.3.0 API Reference Manual.html

Once web page open, then click the on the "Architectural Overview" from panel on the left and scroll down to read about HAL and Peripheral Drivers.

If you don't want to download and install KSDK_1.3 here is the summary from that document:

Hardware Abstraction Layer (HAL)

The KSDK HAL consists of low-level drivers for the Kinetis MCU product family on-chip peripherals. The main goal is to abstract the hardware peripheral register accesses into a set of stateless basic functional operations. The HAL itself can be used with system services to build application-specific logic or as building blocks for use-case driven high-level Peripheral Drivers. It primarily focuses on the functional control, configuration, and realization of basic peripheral operations. The HAL hides register access details and various MCU peripheral instantiation differences so that, either an application or high-level Peripheral Drivers, can be abstracted from the low-level HW details. Therefore, hardware peripheral must be accessed through HAL.

The HAL can also support some high-level functions with certain logic, provided these high-level functions do not depend on functions from other peripherals, nor impose any action to be taken in interrupt service routines. For example, the UART HAL provides a blocking byte-send function that relies only on the features available in the UART peripheral itself. These high-level functions enhance the usability of the HAL but remain stateless and independent of other peripherals. Essentially, the HAL functional boundary is limited by the peripheral itself. There is one HAL driver for each peripheral and the HAL only accesses the features available within the peripheral. In addition, the HAL does not define interrupt service routine entries or support interrupt handling. These tasks must be handled by a high-level Peripheral Driver together with the Interrupt Manager.

The HAL drivers can be found in the KSDK platform/hal directory.

Feature Header Files

The HAL is designed to be reusable regardless of the peripheral configuration differences from one Kinetis MCU device to another. An overall Peripheral Feature Header File is provided for KSDK-supported MCU device to define the feature or configuration differences for each Kinetis sub-family device.

Design Guidelines

This section summarizes the design guidelines that were used to develop the HAL drivers. It is meant for information purposes and provides more details on the make-up of the HAL drivers. As previously stated, the main goal of the HAL is to abstract the hardware details and provide a set of easy-to-use low-level drivers. The HAL itself can be used directly by the user application; in this case, the high-level Peripheral Drivers that are built on top of the HAL serve as a reference implementation and to demonstrate the HAL usage. The HAL is mainly focused on individual functional primitives and makes no assumption of use-cases. It also implements some high-level functions with certain logic without dependencies from other peripherals and does not impose any interrupt handling. The HAL APIs follow a naming convention that is consistent from one peripheral to the next. This is a summary of the design guidelines used when developing the HAL drivers:

  • There is a dedicated HAL driver for each individual peripheral. Peripherals with different versions or configurations are treated as the same peripheral with differences handled through a feature header file. HAL should hide both the peripheral and MCU details and differences from the high-level application and drivers.
  • Each HAL driver has an initialization function to put the peripheral into a known default state (i.e., the peripheral reset state). There is no corresponding de-initialization function.
  • Each HAL driver has an enable and disable function to enable or disable the peripheral module.
  • The HAL driver does not have an internal operation context and should not dynamically allocate memory.
  • The HAL provides both blocking and non-blocking functions for peripherals that support data transaction-related operations.
  • The HAL may implement high-level functions based on abstracted functional primitives, provided this implementation does not depend on functions outside of the peripheral and does not involve interrupt handling. The HAL must remain stateless.
  • The HAL driver does not depend on any other software entities or invoke any functions from other peripherals.

Peripheral Drivers

The KSDK Peripheral Drivers are use-case driven high-level drivers that implement high-level logic transactions based on one or more HAL drivers, other Peripheral Drivers, and/or System Services. Consider, for example, the differences in the UART HAL and the UART Peripheral Driver. The UART HAL mainly focuses on byte-level basic functional primitives, while the UART Peripheral Driver operates on an interrupt-driven level using data buffers to transfer a stream of bytes and may be able to interface with DMA Peripheral Driver for DMA-enabled transfers between data buffers. In general, if a driver, that is mainly based on one peripheral, interfaces with functions beyond its own HAL and/or requires interrupt servicing, the driver is considered a high-level Peripheral Driver.The KSDK Peripheral Drivers support all instances of each peripheral instantiated on the Kinetis MCU by using a simple integer parameter for the peripheral instance number. Each Peripheral Driver includes a “common” file, denoted as fsl_<peripheral>_common.c (where <peripheral> is the name of the peripheral for which the driver is written). This file contains the translation of the peripheral instance number to the peripheral register base address, which is then passed into the HAL. Hence, the user of the Peripheral Driver does not need to know the peripheral memory-mapped base address.The Peripheral Drivers operate on a high-level logic that requires data storage for internal operation context handling. However, the Peripheral Drivers do not allocate this memory space. Rather, the user passes in the memory for the driver internal operation through the driver initialization function. Note that HAL is used for MCUs with restricted RAM and FLASH size.The Peripheral Drivers are designed to handle the entire functionality for a targeted use-case. An application should be able to use only the Peripheral Driver to accomplish its purpose. The mixing of the Peripheral Driver and HAL by an application for the same peripheral can be done, but is discouraged for architectural cleanliness and to avoid cases where bypassing the Peripheral Driver results in logic errors within the Peripheral Driver.The Peripheral Drivers can be found in the KSDK platform/drivers directory.

Interrupt Handling

Interrupt-driven Peripheral Drivers are designed to service all interrupts for their desired functionality. Each Peripheral Driver implements a set of easy-to-use APIs for a particular use-case. Each Peripheral Driver also exposes interrupt functions that implement all actions taken when serving a particular interrupt. These interrupt action functions take in the peripheral instance number as an input parameter. All Interrupt Service Routine (ISR) entries for the Peripheral Driver are implemented in a separate C file named the fsl_<peripheral>_irq.c, which is located in the top level of the Peripheral Driver folder. The ISR entries invoke a corresponding interrupt action functions that are implemented in the driver and are exposed as part of the driver public interfaces. Each interrupt action function is hard coded with the peripheral instance number. Note that the IRQ file depends on the Peripheral Driver but the driver does not depend on the IRQ file.The CMSIS startup code contains the vector table with the ISR entry names which are defined as weak references. The Peripheral Driver ISR entry names match the names defined in the vector table such that these newly-defined ISR entries in the driver replace the weak references defined in the vector table. There is no dependency on the location of the vector table. However, if the vector table is re-located (normally to RAM), the ISR entry names should remain consistent.Each Peripheral Driver IRQ file defines the ISR entries for all instances of the peripheral instantiated on the MCU. Any unused ISR entries can be safely deleted in the user application. Note that, when building driver libraries for a particular MCU, the IRQ files are not part of the library build. When developing an application, however, include these IRQ files into the application project space.If you want to use the HAL to directly build an interrupt-driven application or a high-level driver, define the ISR entries to service needed interrupts. The ISR entry names have to match the names of the ISR entry names provided in the CMSIS startup code vector table. Normally, the vector table is relocated to RAM during system startup and the ISR entry names remain unchanged. However, should these ISR entry names change, the user is required to register the newly defined ISR entry table names by invoking the Interrupt Manager registration function.When working with an RTOS, if the target operating system has its own interrupt handling mechanism, the user’s ISR has to dynamically register the internal vector table maintained inside the OS via the service routine provided by the OS. Some operating systems do not have dedicated interrupt handling, and no special handling is required. Most of the RTOSes designed for the Cortex-M core use PendSV exceptions for scheduling. The PendSV exceptions are low priority and execute only when all other interrupts have been serviced. There are special cases where interrupt handling prologues and epilogues have to be called at the beginning and at the end of an ISR to inform the OS of the entry and exit of an ISR so that the OS scheduler does not trigger a rescheduling event while the system is servicing interrupts. The OS Abstraction layer provides prologues and epilogues in a uniform API for all supported OS.

Peripheral Driver Types

Peripheral Drivers are designed and operated on use-case driven high-level logic. For that reason, the interaction between a Peripheral driver and other software components has a few limitations. This is a list of typical KSDK Peripheral Driver types to demonstrate this concept:

  • Peripheral Drivers that use one HAL for a particular IP and system services
  • Peripheral Drivers that use multiple HAL components and System Services. An example involves a Peripheral Driver that uses both the DMA HAL and the I2C HAL to build a DMA-enabled high-level I2C driver. At the same time, a DMA Peripheral Driver already exists and provides the overall DMA channel management. In this situation, issues can arise for the dedicated DMA Peripheral Driver because it is unaware of use of resources for the DMA-enabled I2C driver that accesses the DMA HAL directly. In this case, the KSDK Peripheral Drivers will only use the DMA HAL when configuring the DMA Transfer Control Descriptor for a particular channel that is dedicated to the driver and avoid using the DMA HAL to change the DMA peripheral control registers. The DMA channel allocation for a particular Peripheral Driver is normally assigned during the initialization of the peripheral by calling the DMA Peripheral Driver channel request function. In this way, the DMA maintains a used channel registry.
  • Peripheral Drivers that use a combination of HAL, other Peripheral Drivers, and System Services for solution-based composite high level drivers.

Design guidelines

This section summarizes the design guidelines to develop the Peripheral Drivers. In this list, the term Peripheral Driver is replaced with the acronym “PD”:

  • The PD does not directly access hardware registers and only uses HAL to interface with hardware. It uses other PDs indirectly to access hardware functions.
  • The PD does not dynamically allocate memory and does not assume any static configuration at compile-time. It supports run-time configurations by taking in a configuration data structure from the Application in an initialization function. This initialization function also takes in the memory allocated for internal operational context storage needs. The PD only reads from the configuration data structure. The configuration data structure is defined as “const”.
  • The PD supports an initialization function and has a corresponding de-initialization function.
  • The PD supports both blocking and non-blocking functions for data transactions.
  • The PD does not depend on any software or hardware entities that do not relate to any of the peripherals available on the Kinetis platform. For example, the Ethernet (ENET) PD does not depend on an external ENET PHY, even if the ENET PD does not function without an associated external PHY.
  • If the PD is built on top of HAL, the PD can work with any instance of the peripheral by taking the instance number as a parameter. When global data is shared across multiple instances, the global data access has to be protected when working with an RTOS. This can be done using the critical section functions implemented as part of the RTOS abstraction. This data access protection is addressed with the bare-metal OS abstraction implementation when no RTOS is used.
  • When the ISR and other public API functions within the driver access the PD internal operation context, that data must be defined as volatile so that compiler does not inadvertently optimize the code resulting in an undesired functionality.
  • The PD provides enough functions to allow the APIs provided by PD to meet the target use-case implementation. The user application should not mix the use of both a PD and HAL .
  • The PD does not configure pin muxing or set up interrupt priorities for related interrupts. Those items are handled by the board-specific configuration and the application-specific logic.

Regards,

David

0 项奖励
回复