Freertos uart receive

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Freertos uart receive

3,429件の閲覧回数
wyao75
Contributor I

Hi

I use the SDK_2.2_TWR-K60D100M and try to use the freertos_uart.c on my TWR-K60D100M board to test receive data from UART. 

The program like this 

   UART_RTOS_Receive(&handle, recv_buffer, 20, &n);

   if(n==20)

      UART_RTOS_Send(&handle, (uint8_t *)recv_buffer, n);

Now, I use the labtop send data to TWR-K60D100M board.

I found when the program run to UART_RTOS_Receive(&handle, recv_buffer, 20, &n), the program is going to block state, when receive data over 20 and the program will active.

My question is how to let the UART_RTOS_Receive(&handle, recv_buffer, 20, &n) immediately return, rather than wait the received data over 20. 

 

0 件の賞賛
返信
3 返答(返信)

2,726件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi 姚 &#29614

RTOS Uart driver is blocking the current task until whole required data are received. Please check the API UART_RTOS_Receive.

int UART_RTOS_Receive(uart_rtos_handle_t *handle, uint8_t *buffer, uint32_t length, size_t *received).

In your case, you specify the number of data words as 20. If you define the length as 1, the function will receive just 1 byte every time and return immediately.


Have a great day,
Daniel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,726件の閲覧回数
chinagkuanyi
Contributor I

I have same question, any update? I want receive non block data

0 件の賞賛
返信

2,726件の閲覧回数
sreejithmenon
Contributor I

What if i am streaming some data to the UART. I would like to use the RTOS UART DRIVER and process lets say 20 data word blocks, except that the last packet is only 8 words and i need to process it.Any suggestions as to how to handle this.

Thanks

0 件の賞賛
返信