Freemaster with MKM34

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Freemaster with MKM34

2,004件の閲覧回数
dhruvonline
Contributor III

Hi Martin,

I have to use the UART3 for Freemaster for Energy, Current and Voltage and Reading in the 3-Phase Energy Meter. 

As per the MKM reference design, UART2 is used for that. Can you suggest the changes required at Meter side and PC side?

Regds,

Dhruv

0 件の賞賛
返信
2 返答(返信)

1,823件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Dhruv,

Pls refer to the application note an4752, it is helpful to understand how to change the uart module.

https://www.nxp.com/docs/en/application-note/AN4752.pdf 

BR

Xiangjun rong

0 件の賞賛
返信

1,823件の閲覧回数
dhruvonline
Contributor III

Hi xiangjun.rong,

Thanks for the suggestion. I will check it.

Regds,

Dhruv

0 件の賞賛
返信