FreeRTOS + interrupt handling using KSDK 1.2.0 / KDS 3.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FreeRTOS + interrupt handling using KSDK 1.2.0 / KDS 3.0

2,442件の閲覧回数
Kewal
Contributor IV

I have been trying to get the interrupt working. Just a simple interrupt from a switch. As I am using safeRTOS instead of FreeRTOS which is a similar component but not same. OSAL layer for hte safeRTOS has been defined properly. The port interrupts are getting called but not able to really get an interrupt on a specific pin. To an extent, not able to pin down on the issue right now. Any guides or documentation which figures out interrupt mechanism on FreeRTOS would help.

 

Thanks.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,000件の閲覧回数
Kewal
Contributor IV

I have actually configured the event to generate code for that particular interrupt. Now that I am seeing the error as  belowUntitled.png

Also, I am using IAR embedded workbench 7.2 to build my own project file with all the generated the source code from KDS (PE).

0 件の賞賛
返信

2,000件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Kewal,

A quick test that can be done is inherent (but hidden) within KSDK_1.3 FreeRTOS power manager rtos demo.

C:\Freescale\KSDK_1.3.0\examples\twrk65f180m\demo_apps\power_manager_rtos_demo\power_manager_rtos_demo_freertos\iar

This example already sets up an interrupt handler for a push button switch on the board.

It takes some digging to find where all the magic is happening and making a small code edit too.

In board.h I had made edit:

#define BOARD_SW_NAME               "SW3"//DES was "SW1"

In gpio_pins.c I enable the interrupt for kGpioSW1 (which really is SW3 on the twrk65f180m):

const gpio_input_pin_user_config_t switchPins[] = {

  {

    .pinName = kGpioSW1,

    .config.isPullEnable = true,

    .config.pullSelect = kPortPullUp,

    .config.isPassiveFilterEnabled = false,

    .config.isDigitalFilterEnabled = false,

    .config.interrupt = kPortIntFallingEdge                //DES was kPortIntDisabled

  },

In gpio_pins.h header comments added:

enum _gpio_pins_pinNames{

    kGpioSW1 = GPIO_MAKE_PIN(GPIOA_IDX, 10U), //DES SW3 on TWR-K65F180M Rev D

    kGpioSW2 = GPIO_MAKE_PIN(GPIOA_IDX, 4U), //DES SW2 on TWR-K65F180M Rev D

...

Also in this header is following renaming:

#define BOARD_SW_LLWU_IRQ_HANDLER    PORTA_IRQHandler

The PORTA_IRQHandler is a default that is weakly defined in startup_MK65F18.s file.  When you implement the same name function in your application code you are overloading the function and it will be used.  This happens in task_lpm.c.

In task_lpm.c is where the Interrupt handler has been defined for the power management demo but it also will clear the GPIO Port A interrupt flag (Note Any interrupt for Port A pins go to one interrupt routine and that routine if more robust would determine which pin was the interrupt source but our demo doesn't do that).

/* IRQ handler for switch/button. */

void BOARD_SW_LLWU_IRQ_HANDLER(void)

{

#if 1           //DES 0=test, 1=default code

    PORT_HAL_ClearPortIntFlag(BOARD_SW_LLWU_BASE);

#else

    GPIO_DRV_ClearPinIntFlag(kGpioSW1);         //DES added...this does work too and the two statements are equivalent

#endif

}

Regards,

David

0 件の賞賛
返信