First test of SDK Project Genrator

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

First test of SDK Project Genrator

2,849件の閲覧回数
miltonsierra
Contributor II

If you go to the link of freedom board K64F http://www.freescale.com/frdm-k64f , you will find a new step by step tutorial for begin to program with Kinetis using a software tool "SDK Project Generator".

pagefrdk.png

Freescale Freedom Development Platform for Ki|Freescale

pagefrdk2.png

 

I have created a project using the SDK Project Generator and my project was automatically located in <SDK_Install_Directory>/examples/frdmk64/user_apps. 

pro2.png

In my opinion the SDK project generator is a quick way to begin to program and not lose the time making settings of linker files.

ラベル(1)
4 返答(返信)

2,437件の閲覧回数
neilhancock
Contributor IV

FYI, just tried this on KSDK 1.3.0 and says not supported.

I have been using the tool for KSDK 1.2.0 so downloaded again, and the file size is the same so I'm guessing its the same tool.

pastedImage_0.png

2,437件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi Neil,

yes, you are absolutely correct.

The current version of Project Generator Beta does not support KSDK 1.3.

We expect new version for KSDK Project Generator in these two weeks.

Thank you for your interest and for this valuable contribution!

I hope this helps you.

Best Regards,

Iva

2,437件の閲覧回数
EmanueleB
Contributor I

Hi Iva, do You have any news about new project generator version?

Kind regards,

EB

0 件の賞賛
返信

2,437件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi Emanuele,

yes, KSDK Project Generator is available now! You can download it from here Software Development Kit for Kinetis MCUs|Freescale

Please, look at the article here New Kinetis SDK Project Generator is available!

Wish it helps.

-Iva

0 件の賞賛
返信