FTM_StartTimer does not start Timer KSDK2.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FTM_StartTimer does not start Timer KSDK2.0

1,567 次查看
manfredschnell
Contributor IV

Hello,

 

I use KSDK2.0 with IAR Workbench on Target K64.

With FTM-Modul I want to generate triac firing pulses for phase angle Modulation.

 

So I use the following sequence.

 

#define BOARD_PWM_INSTANCE_50HZ               FTM3

// PWM-Modul Init 50Hz

  FTM_GetDefaultConfig(&ftmInfo);

  // Initializes the FTM module.

  ftmInfo.prescale = kFTM_Prescale_Divide_8;

  FTM_Init(BOARD_PWM_INSTANCE_50HZ, &ftmInfo);

  FTM_SetupOutputCompare( BOARD_PWM_INSTANCE_50HZ, BOARD_PWM_TRIAC1_CH, kFTM_NoOutputSignal, 0 );

  FTM_StartTimer(BOARD_PWM_INSTANCE_50HZ, kFTM_SystemClock);

 

After that sequence the FTM-module does not count.

I have to write a value (0xffff --> to have a free running Counter) to "MOD" register.

BOARD_PWM_INSTANCE_50HZ->MOD = 0xffff;

 

The reason is written in "K64 Sub-Family Reference Manual, Rev. 2, January 2014" on page 1007.

"...

 

• When MOD = 0x0000, CNTIN = 0x0000, for example

 

after reset, and FTMEN = 1, the FTM counter remains

 

stopped at 0x0000 until a non-zero value is written into the

 

MOD or CNTIN registers.

 

..."

 

The Function FTM_StartTimer() works, when the timer is used in PWM-mode with FTM_SetupPwm() because the "MOD" register is written in this function to adjust the PWM frequency.

 

Best Regards

Manfred

标签 (1)
0 项奖励
回复
0 回复数