Example using LCD TFT ILI9341

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example using LCD TFT ILI9341

4,751件の閲覧回数
jordangarcia
Contributor II

Hey guys;

 

 

Is there an example using LCD TFT ILI9341?

 

I´m new "playing" with it, if you have any information about

how to "play it". it would great to me.

 

I´m using KDS&SDK but I can use Codewarrior, and I use frdm-k64

but I just need an example, any uC is ok.

 

Thanks;

 

Jordan c:

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,983件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello Jordan Garcia,

no, we have examples for TWR-LCD (Graphical LCD Tower System Module),based on SSD LCD driver, Graphical LCD Tower System Module|Freescale

If you want to make this demo, I recommend to download the driver from internet (written in C language) for this display

and then rewrite low level layer (SPI) on freescale SPI driver - or you can use SPI KSDK driver.

I hope this helps,

Best Regards,

Iva

2,981件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

This is IL9341 driver for eGUI . https://github.com/Gargy007/eGUI

Luis

0 件の賞賛
返信