EmbSys Viewer will not Install on Luna 4.4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EmbSys Viewer will not Install on Luna 4.4

8,208件の閲覧回数
bcstewart
Contributor III
I have tried to install EmbSys Viewer on KDS 3.2 with Luna 4.4.
I followed the methods described in this forum and on mcuoneclipse.com

When I try to specify the device (K22F), NXP or Freescale is not listed in the vendor listing.

Any suggestions?
 
pastedImage_6.png

0 件の賞賛
返信
7 返答(返信)

7,995件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Are the NXP/Freescale SVD files present in your data files/collection for EmbSysRegView?

Depending on your EmbSysRegView, this might be different, see Adding CMSIS-SVD Files to EmbSysRegView 0.2.6.r192 and Eclipse | MCU on Eclipse 

I hope this helps,

Erich

0 件の賞賛
返信

7,990件の閲覧回数
bcstewart
Contributor III

OK.  I see it in the ADV(CMSIS) folder.  But KDS is not recognizing it.

0 件の賞賛
返信

7,990件の閲覧回数
BlackNight
NXP Employee
NXP Employee

I think you mean the 'SVD(CMSIS)' folder. Not sure why it does not list it for you. But in any case, you can pick and choose any folder name or move files into a folder of your choice inside the data.

0 件の賞賛
返信

7,990件の閲覧回数
bcstewart
Contributor III

Yes, it's installed.

But if you look at the package, NXP is missing!  (note:  I temporarily

renamed the .jar to .zip)

Very strange...

--Brad

0 件の賞賛
返信

7,990件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Can you check the SVD folder in that zip file?

0 件の賞賛
返信

7,990件の閲覧回数
bcstewart
Contributor III

Working now.

Simply need to select SVD(CMSIS) under Architecture in the EmbSysReg

section and then select Freescale.  A bit different approach from the

article since I didn't create a KDS directory and copy the files.  This

is not easy if you don't have Winzip Pro.  So I simply left it as is.

0 件の賞賛
返信

7,990件の閲覧回数
BlackNight
NXP Employee
NXP Employee

You don't need WinZip Pro. Any zip tool (as 7-Zip) can do this.

0 件の賞賛
返信