Does anybody have experience with the Zephyr Micro/Nano RTOS?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does anybody have experience with the Zephyr Micro/Nano RTOS?

Jump to solution
1,248 Views
myke_predko
Senior Contributor III

Gentlebeings,

 

I just saw this announcement (http://linuxgizmos.com/zephyr-a-tiny-open-source-iot-rtos/) on Slashdot discussing the Zephyr RTOS (https://www.zephyrproject.org/content/zephyr-kernel-v100-release-notes).  What caught my eye is that a) it's been implemented for the FRDM-K64F and b) that it can be as small as 10k. 

 

I'm experimenting with freeRTOS and for my product, I want to use it along with USB CDC or HID and the FatFs on a 128k Flash sized K22F and things are looking very tight for implementing logic with it. 

 

Thanx,

 

myke

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
743 Views
Jmart
NXP Employee
NXP Employee

Myke,

As you can imagine, Zephyr is still in its infancy. The 1.0 push that is now accessible does have some K64 support, but it's far from a full platform at this time. I'd continue down the FrerRTOS path that you're on for now and keep an eye on Zephyr as it matures.

Jason

View solution in original post

0 Kudos
Reply
2 Replies
744 Views
Jmart
NXP Employee
NXP Employee

Myke,

As you can imagine, Zephyr is still in its infancy. The 1.0 push that is now accessible does have some K64 support, but it's far from a full platform at this time. I'd continue down the FrerRTOS path that you're on for now and keep an eye on Zephyr as it matures.

Jason

0 Kudos
Reply
743 Views
myke_predko
Senior Contributor III

Okay - Thanx!

0 Kudos
Reply