Default_ISR during KSDK initialization

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Default_ISR during KSDK initialization

1,838件の閲覧回数
MAPC
Senior Contributor I

Hello

 

My customer is working on a project with MK22FN256 and we are facing a strange problem. We noticed that we always fall into an unhandled interrupt service routine "Default_ISR", but we have no idea of what is causing it and we don't know how to see it in KDS Debugger.

 

His project is bare-metal and doesn't use Processor Expert.

 

We carefully checked out his intialization code, but we didn't see anything wrong. Default_ISR is always called at the same point in the firmware, no matter if we add or remove lines. So, any ramdom event may be causing this interrupt. Even if we disable global interrupts, the problem remains.

 

Can anybody help us on that please?

 

Bellow, we post a video showing the problem. Here you can see Default_ISR happens as we enter "CLOCK_SYS_EnableRtcClock" function, but if we insert some lines with "nop", for example, it change the point.

 

outdiv - YouTube

 

Have attached his project, for analysis purpose.

 

Thanks,

 

Marco Coelho

Applications Engineer

Siletec Eletronica

Original Attachment has been moved to: Cain_V03_00_00.rar

ラベル(1)
0 件の賞賛
返信
1 返信

1,673件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Marco,

Whether the is the hardware problem , doest the 32.768 RTC work well ?

I have test you project on FRDM-K22f board , the chip is MK22FN512, it work well .

On first  built , there have one simple project , after i include the header file "#include "gpio_pins.h"" on the

file of "trata_teclas.c" , it can work well .

I also take a screenshot about single-step debug , you can check it can run well on the function of "CLOCK_SYS_EnableRtcClock" .

So i please check the hardware , you can refer to the sch of frdm-k22f.

pastedImage_0.png

pastedImage_1.png

pastedImage_2.png

pastedImage_3.png

pastedImage_4.png

pastedImage_5.png

pastedImage_6.png

Hope it helps

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------


Have a great day,
Alice Yang

0 件の賞賛
返信