Client include-paths

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Client include-paths

2,056 次查看
oaf
Contributor IV

Hi,

 

KDS-3.0, KSDK-1.2.0

I wonder which include files are intended for application programmers. Is there any rule to use?

Today I want to use 'shell.h' which is located in 3 places:

    1. rtos\mqx\lib\frdmk64f.kds\debug

    2. rtos\mqx\nshell\source

    3. utilities

标签 (1)
标记 (2)
0 项奖励
回复
3 回复数

1,933 次查看
ivadorazinova
NXP Employee
NXP Employee

Hello Ole Asbjorn Fadum,

in shell.h located at \utilities\shell\ you set general settings.

in shell.h located at \rtos\mqx\nshell\source\include\ you set MQX RTOS nShell.

Best Regards,

Iva

0 项奖励
回复

1,933 次查看
oaf
Contributor IV

Hi,

And which one should my project include?

0 项奖励
回复

1,933 次查看
ivadorazinova
NXP Employee
NXP Employee

Hello Ole,

please, modify files in this folder. It depends what do you exactly want to modify if you need to add command, change command behavior etc...

shell.png

I hope this helps,

Best Regards
Iva

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复