Chip Specific Configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Chip Specific Configuration

跳至解决方案
2,378 次查看
knishi
Contributor I

Hi, community.

 

Where could we find the ACTUAL meaning for the enum variable that explained as chip-specific on the SDK API manual?

For example, if I check the kPort_MuxAlt2 (which explained as chip specific), I tried to find the EXPLICIT explanation *(such as kPort_MuxAlt2: use for something) when and how I will use this value on either SDK API manual and reference manual for the chip.

 

Unfortunately, the Kinetic expert pin configuration tool is not compatible for the chip I am testing right now.

 

Is there any single document with explicit explanation to find the function on the specific chip?

 

Thank you for your help in advance.

标签 (1)
0 项奖励
回复
1 解答
2,209 次查看
DavidS
NXP Employee
NXP Employee

Hi Kazunori,

The Kinetis MCU Reference Manual's Chapter 10 "Signals Multiplexing and Signal Descriptions" has a table to show the multiplexing on each pin and it is the "ALTn" parameter that is used to select the desired pin functionality.

Example from the K64P144M120SF5RM_Rev2.pdf:

pastedImage_1.png

Regards,

David 

在原帖中查看解决方案

2 回复数
2,210 次查看
DavidS
NXP Employee
NXP Employee

Hi Kazunori,

The Kinetis MCU Reference Manual's Chapter 10 "Signals Multiplexing and Signal Descriptions" has a table to show the multiplexing on each pin and it is the "ALTn" parameter that is used to select the desired pin functionality.

Example from the K64P144M120SF5RM_Rev2.pdf:

pastedImage_1.png

Regards,

David 

2,209 次查看
knishi
Contributor I

Thank you, David.

That is what I am looking for.

Regards

0 项奖励
回复