Bug in _mqx_init_interrupt_stack() when using bootloader (KSDK 1.2.0)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Bug in _mqx_init_interrupt_stack() when using bootloader (KSDK 1.2.0)

1,238 次查看
priya_dwivedula
Contributor III

I found a bug in _mqx_init_interrupt_stack() routine where the stack base address is obtained from this line of code.
stack_ptr = (_mqx_uint)*(_mqx_uint*)0x0; /* Get stack base address located on interrupt vector 0. */

 

Since the interrupt vector relocates to a different address (for instance, 0xa000) when using a bootloader, the above line would result in an incorrect value for stack_ptr which in turn results in incorrect INIT.INTERRUPT_STACK_SIZE. This was causing a hard-fault in my case when _sched_start_internal() is called. The right way to fix it is to get the stack base address from VTOR as below.

stack_ptr = (_mqx_uint)*(_mqx_uint*)SCB->VTOR;

 

By the way, I was using FRDM-K22F board with freedom bootloader to debug this issue and I also noticed that this issue is fixed in KSDK 1.3.0.

 

Thanks,
Priya

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,113 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi Priya,

Thank you for your feedback.

This issue should be fixed in KSDK 1.3.

Have a great day!

Iva

0 项奖励
回复