Brief Introduction to LwIP stack in MCUXpresso SDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Brief Introduction to LwIP stack in MCUXpresso SDK

Brief Introduction to LwIP stack in MCUXpresso SDK

LwIP is a small independent implementations of the TCP/IP protocol suite that has been initially developed by Adam Dunkels . The focus of the lwIP TCP/IP implementation is to reduce resource usage while still having a full scale TCP. This makes lwIP suitable for use in embedded systems with tens of kilobytes of free RAM and room for around 40 kilobytes of code ROM. 

Currently LwIP 2.1.2 is ported to Kinetis and I.MX RT families in MCUXpresso SDK 2.6 .

Features:

LwIP comes with the following protocols:

IPv4 and IPv6, including packet forwarding over multiple network interfaces.

ICMP for network maintenance and debugging

IGMP for multicast traffic management

MLD (Multicast listener discovery for IPv6). 

ND (Neighbor discovery and stateless address autoconfiguration for IPv6)

DHCP and DHCPv6.

UDP (User Datagram Protocol)

TCP (Transmission Control Protocol)

Raw/native API for enhanced performance

Optional Berkeley -  like socket API.

TLS: optional layered TCP for nearly transparent TLS for any TCP-based protocol

PPPoS and PPPoE

DNS (Domain name resolver incl. mDNS)

6LoWPAN

Organization of the LwIP stack

Let’s take SDK_2.6.1_EVKB-IMXRT1050 for example,

LwIP code in under SDK_2.6.1_EVKB-IMXRT1050\middleware\lwip

pastedImage_1.png

Port: This folder includes the adapter code which can make the LwIP stack run on the bare metal and FreeRTOS.

pastedImage_2.png

Enet_ethernetif.c/h: Adapt the LwIP stack to the underlying MCUXpresso SDK ethernet driver, provides ethernet interfaces , like  phy init and  ethernetif_input.

cc.c/h: provide typedefs, compiler hints for packing and platform specific diagnostic output.

Perf.h: architecture specific performance measurement, current the definitions is NULL, reserve for future use.

Src: This folder includes the latest stable LwIP 2.1.2 source code which can be downloaded from below link download.savannah.gnu.org/releases/lwip/

--api: netconn and socket API files

--core: LwIP core files

--include: LwIP include files

--netif:  network interface files

LwIP APIs overview

LwIP provides three application programming interfaces (API) for programmers to use for communication with the TCP/IP code:

Raw APIs:   Non thread-safe APIs, callback style for maximum performance and minimum memory footprint. Program execution is driven by callbacks functions, which are then invoked by the lwIP core when activity related to that application occurs. A particular application may register to be notified via a callback function for events such as incoming data available, outgoing data sent, error notifications, poll timer expiration, connection closed, etc. An application can provide a callback function to perform processing for any or all of these events.

Sequential-style APIs:    blocking functions. More overhead, but can be called from any thread except TCPIP thread. The sequential API provides a way for ordinary, sequential, programs to use the lwIP stack. It is quite similar to the BSD socket API. The model of execution is based on the blocking open-read-write-close paradigm. Since the TCP/IP stack is event based by nature, the TCP/IP code and the application program must reside in different execution contexts (threads).

Socket API: BSD-style socket API.  The socket API is a compatibility API for existing applications, currently it is built on top of the sequential API. It is meant to provide all functions needed to run socket API applications running on other platforms.

TCP Raw API

 

API function

Description

TCP connection setup

 

tcp_new()

Creates a new TCP PCB

tcp_bind()

Binds a TCP PCB to a local IP address and port

tcp_listen()

Starts the listening process on the TCP PCB.

tcp_accept()

Assigns a callback function that will be called when a

new TCP connection arrives.

tcp_connect()

Used to connect to a remote TCP host.

Sending TCP data

tcp_write()

Queues up data to be sent.

tcp_output()

Forces queued data to be sent

tcp_sent()

Assigns a callback function that will be called when sent

data is acknowledged by the remote host.

Receiving TCP data

tcp_recv()

Sets the callback function that will be called when new

data arrives.

tcp_recved()

Must be called when the application has processed the

incoming data packet (for TCP window management).

Application polling

tcp_poll()

Assigns a callback functions that will be called

periodically. It can be used by the application to check if

there is remaining application data that needs to be sent

or if there are connections that need to be closed.

Closing and aborting connections

tcp_close()

Closes a TCP connection with a remote host.

tcp_abort()

Aborts a TCP connection.

tcp_err()

Assigns a callback function for handling connections

aborted by the lwIP due to errors (such as memory

shortage errors).

UDP Raw API

API

Description

udp_bind

Binds a UDP PCB with a local IP address and port.

udp_new

Creates a new UDP PCB.

udp_send

Sends UDP data.

udp_recv

Specifies a callback function which is called when a datagram is received

udp_remove

Removes and de-allocates a UDP PCB.

udp_connect

Sets up a UDP PCB remote IP address and port

udp_disconnect

Removes a UDP PCB remote IP and port.

Netconn API

netconn_new

Creates a new connection

netconn_listen

Sets a TCP connection into a listening mode

netconn_write

Sends data on a connected TCP netconn

netconn_accept

Accepts an incoming connection on a listening TCP connection

netconn_close

Closes a TCP connection without deleting it.

netconn_send

Sends data to the currently connected remote IP/port (not applicable for

TCP connections).

netconn_bind

Binds a connection to a local IP address and port.

netconn_recv

Receives data from a netconn.

netconn_connect

Connects to a remote IP address and port.

 

Socket API

Macro

API

description

accept

lwip_accept

Accepts a new connection on a socket

bind

 lwip_bind

Binds a socket to an IP address and port

shutdown

 lwip_shutdown

 

getpeername

 lwip_getpeername

 

getsockname

lwip_getsockname

 

setsockopt

lwip_setsockopt

 

closesocket

 lwip_close

 

connect

lwip_connect

Connects a socket to a remote host IP address and port.

listen

 lwip_listen

Listens for socket connections

recv

 lwip_recv

 

recvmsg

lwip_recvmsg

 

recvfrom

 lwip_recvfrom

 

send

 lwip_send

 

sendmsg

 lwip_sendmsg

 

sendto

lwip_sendto

 

socket

 lwip_socket

Creates an new socket.

poll

lwip_poll

 

ioctlsocket

lwip_ioctl

 

inet_ntop

 lwip_inet_ntop

 

inet_pton

 lwip_inet_pton

 

read

 lwip_read

Reads data from a socket

readv

lwip_readv

 

write

lwip_write

Writes data on a socket

writev

lwip_writev

 

close

 lwip_close

Closes a socket (socket is deleted).

fcntl

 lwip_fcntl

 

ioctl

lwip_ioctl

 

 

 

 

LwIP Configure

Configuration file is placed in application source folder: Lwipopts.h:

pastedImage_3.png

Lwipopts.h is a user file that you can use to fully configure LwIP and all of it’s modules. You do not need to define every option that LwIP provides; if you do not define an option, a default value will be used. Therefore, your lwipopts.h provides a way to override much of the behavior of LwIP.

LwIP Demos in MCUXpresso SDK

MCUXpresso SDK comes with lots of demos that use different API sets.

Name

Description

Lwip_tcpecho

a TCP echo demo on the lwIP TCP/IP stack with bare metal KSDK or FreeRTOS. The demo uses the TCP protocol and acts as an echo server

Lwip_udpecho

a UDP echo demo on the lwIP TCP/IP stack with bare metal KSDK or FreeRTOS, which uses the UDP protocol and acts as an echo server.

Lwip_ping

a Ping Demo on the lwIP TCP/IP stack which using the ICMP protocol

lwip_nghttp2cli_mbedTLS

an NGHTTP2 client set up on lwIP TCP/IP and the MbedTLS stack with

FreeRTOS

lwip_mqtt

MQTT client connecting to MQTT broker via unsecured socket

lwip_iperf

check your bandwidth using the network performance measurement IPerf application on a PC as a client or a server

lwip_httpsrv

an HTTPServer on the lwIP TCP/IP stack with bare metal SDK or FreeRTOS

lwip_httpscli_mbedTLS

an HTTPS client set up on lwIP TCP/IP and the MbedTLS stack with

FreeRTOS

lwip_dhcp_usb

a DHCP and ping demo on the lwIP TCP/IP and USB stack

lwip_dhcp

a DHCP client and prints the status as it is progressing

評価なし
バージョン履歴
最終更新日:
‎11-04-2019 08:09 AM
更新者: