An example project for FIR function implement on KV31 with SDK and CMSIS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

An example project for FIR function implement on KV31 with SDK and CMSIS

An example project for FIR function implement on KV31 with SDK and CMSIS

This example project shows how to use CMSIS DSP functions to implement a digital filter. The project is based on Kinetis KV31F512.

 

It first generates a mixed signal which is composed by two sine waves.  Then it uses PDB to trigger DAC every 200 microsecond and output the signal through DAC, so that the mixed signal can be displaying on oscilloscope.

 

With QEDesign tool, a lowpass filter is designed, the filter coefficients are used directly to initialize the FIR function supplied by CMSIS DSP library.

This example calls the FIR functions in CMSIS DSP lib, and the filtered signal is output though DAC module.

ラベル(1)
添付
評価なし
バージョン履歴
最終更新日:
‎09-28-2015 03:12 AM
更新者: