ADC multi ch with DMA on KL27

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC multi ch with DMA on KL27

1,298 Views
shuichiy
Contributor III

Hi, I'm now working on KL27Z256 with KSDK2.0.

My goal is to get 5ch data via ADC with DMA transfer.

 

I think 5*16bit ADC0-RA data should be stored in memory in a row, and ADC0->SC1 is switched automatically.

In my codes attached, only the first 16bit data is stored in memory even if ADC0->SC1 seems to be changed.

 

Unfortunately I haven't found any sample codes  on the SDK and here.

Is there something wrong ?

Your any advice will be appreciated.

Original Attachment has been moved to: dma_peripheral_to_memory.c.zip

0 Kudos
Reply
2 Replies

1,039 Views
shuichiy
Contributor III

Thank you for your reply.

I have finally fixed the problem. I needed to change parameters for sc1.

Now, DMA doesn't work again after merging "usb cdc vcom lite" sample into the project but It should be another issue.

0 Kudos
Reply

1,039 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Shuichiy,

I think the solution is okay to use ADC to trigger DMA_CH0, then use channel link(DMA_CH1) to transfer adctable[] to ADC_SC1A to start another ADC conversion.

I think you have to use debugger to display the DMA register setting, especially DMA_DCR0 reg,the LINKCC bits should be 2b'10, the LCH1 bits should be 2b'01.

Pls paste the DMA register setting so that we can have a review.

BR

Xiangjun Rong

0 Kudos
Reply