Spread Spectrum PWM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Spread Spectrum PWM

2,065件の閲覧回数
geoffreylansber
Contributor I

Does the KMS support spread spectrum PWM?   Has anyone attempted to modulate the pwm frequency to spread out the switching noise?

ラベル(1)
0 件の賞賛
返信
1 返信

1,724件の閲覧回数
linestream-adam
Senior Contributor I

Geoffrey,

KMS doesn't feature spread spectrum PWM by default.  You should be able to add support for this into KMS.  You would do this by replacing the SVPWM block with a new block of your own design.

KMS sets up the PWMs to be center-aligned so that the ADC sample is taken in the middle of the PWM period.  So the ADC sample would occur in the same place regardless if the frequency is changing.  In addition to modifying the frequency, you would also need to change the deadtime counter since the FlexTimer handles the deadtime insertion.

I don't think varying the PWM frequency by a few kHz would impact the control loops within KMS.

0 件の賞賛
返信