Sensless position control FRDM-KV31F

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sensless position control FRDM-KV31F

1,568 Views
andreaswickstrom
Contributor II

Hi

Is there any example where i can use a pmsm motor and position control with the   FRDM-KV31F board? 

I can run the sensless velocity but i cant find any example with go to angle. 

I use a motor with a gearbox connected to it.

Best regards

Andreas

Labels (1)
0 Kudos
Reply
1 Reply

1,410 Views
linestream-adam
Senior Contributor I

Andreas,

Kinetis Motor Suite includes a sensored position control reference project. This project requires the use of an encoder attached to the motor. Sensorless control isn't good enough at low speeds to support sensorless position control.

0 Kudos
Reply