Hello,
I had a question about a few of the KMS faults I cannot find in the sensored or sensorless velocity projects, and the Reference Manual does not give me a very good description of these faults. I am using my own hardware, not the development kit, so if some of these faults don't apply with my own hardware please let me know. If you could tell me or point me to where to find the threshold for the faults, what the faults are, and are triggered by. I need to test for each of the faults in my system, if possible, and need to know the thresholds for each, and have a good understanding on how each is set.
These are the faults I cannot find in my project that I may need to test for:
Faults I maybe cannot test for, but just would like to know how they are triggered:
Thanks for the help!
Derek,
All of the faults in KMS are tested for in open code. Most of the faults you have called out are not implemented, the notable exception is the preDriver* faults. They are called out in the header files to reserve the space for future functionality (or if customers want to implemented the fault on their own).
The preDriver* faults are implemented but only in the TWR projects since it's predriver chip reports that fault information back to KMS.
Thanks Adam, so the faults I listed, such as the motor imbalance or open phase are not implemented?
That is all I was checking.
The following faults are not implemented:
Thanks Adam