Running Self-Commisioning Mode from the Command Line

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Running Self-Commisioning Mode from the Command Line

1,500 Views
derekcook
Senior Contributor I

Hello, 

Is it possible to run the self-commissioning user state from the command line to get motor auto-tuning parameters on my own hardware? 

Thanks, 

Derek

Labels (1)
0 Kudos
Reply
2 Replies

1,386 Views
derekcook
Senior Contributor I

Hey Adam, 

Thanks for the reply. I see how to do that now and will let you know if I have any questions.

0 Kudos
Reply

1,386 Views
linestream-adam
Senior Contributor I

Derek,

Yes.  Check out the Lab Guide.  There is a procedure for doing exactly that in there.  If your hardware can communicate to the KMS GUI, it can still do the complete autotuning on custom hardware.

0 Kudos
Reply