Motor Control with FRDM-GD3000EVB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Motor Control with FRDM-GD3000EVB

3,497 Views
DBanks60
Contributor I

I am designing a brushless DC motor control electronics assembly, and I am conducting bench testing with a hardware setup consisting of a FRDM-MC LVMTR, a FRDM-KV31F, a FRDM-GD3000EVB, and a FRDM-PWRSTG1EVB. I'd like to use MCUXpresso for the IDE and find a project to instantiate on the hardware and evaluate the motor performance, but I have not met with success.

Right now I'm trying to use I'm using the project frdmkv31f_mc_bldc, but all I get is a blinking red D4 LED, and no motor movement. 

I'm the electronics hardware engineer on the project (very little software experience), and I only need to spin the motor (under any type of control), verify that the hardware and IDE toolchain will meet our needs, and then I can pass it all along to our software engineers.

Their IDE of choice is MCUXpresso.

Can anyone provide guidance? Thanks!

0 Kudos
Reply
1 Reply

3,487 Views
_Leo_
NXP TechSupport
NXP TechSupport

Hello Dick Banks,

I see that you have another case with the same question, I will follow up on this last one that I mention.

0 Kudos
Reply