MCUXpresso problem opening KMS project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso problem opening KMS project

Jump to solution
2,448 Views
PaulTan
Contributor III

I'm using KMS that successfully characterized a motor, and I told it to export the project.  Now, the question is, am I supposed to be using MCUXpresso or Kinetis Design Studio to compile the project?  

When I use MCUXpresso I get the following error:

MCUXpresso-KMS-Problem1.PNG

So, the question is, am I going down the correct path?  Or should I be using KDS?  And what do I do to fix this error?

Thanks,

Paul Tan.

Labels (1)
0 Kudos
Reply
1 Solution
2,196 Views
PaulTan
Contributor III

Nevermind, found solution - install SDK from Welcome | MCUXpresso SDK Builder 

Also, followed MCUXpresso IDE - Importing MCUXpresso SDK|NXP 

Putting this up in case other people run into the same problem.

Paul Tan.

View solution in original post

0 Kudos
Reply
2 Replies
2,197 Views
PaulTan
Contributor III

Nevermind, found solution - install SDK from Welcome | MCUXpresso SDK Builder 

Also, followed MCUXpresso IDE - Importing MCUXpresso SDK|NXP 

Putting this up in case other people run into the same problem.

Paul Tan.

0 Kudos
Reply
2,196 Views
philip_drake
NXP Employee
NXP Employee

With KMS 1.2 the only time you will need KDS is if you choose an ACIM motor type using the HVP (high voltage platform).  I don't this option is in very high demand as there are no-HVP KV31 or KV46 eval boards out to support that option yet.

Philip

0 Kudos
Reply