MCUXpresso Integrated Development Environment (IDE)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso Integrated Development Environment (IDE)

2,039 Views
toanv
Contributor I

Does the MCUXpresso Integrated Development Environment (IDE) support the build of the TWR-KV10Z32 board demos? Or do I need the IAR tool?

Thanks,


Toan

Labels (1)
0 Kudos
Reply
1 Reply

1,771 Views
philip_drake
NXP Employee
NXP Employee

The easiest way to find out if a board is going to be supported is to go to the MCUXpresso build and request a build of that board.  If it's list, and the TWR-KV10Z32 is listed then you are good to go.

sdk_kv10_twr.png

The TWRKV10Z is not supported by KMS though. I say this because you are in the Kinetis Motor Suite Community post area.

Regards,

Philip

0 Kudos
Reply