KMS GUI command set and syntax

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KMS GUI command set and syntax

2,131 Views
M_Grillo
Contributor III

Hello, Is there a publicized KMS UART command set and syntax requirement/example document for the KV31? I’d like to multipurpose UART0 for the KMS-GUI, our own command set and possibly our own automated configuration setup/monitoring like the KMS GUI in a production piece of test equipment.

 

Thanks,

Mark

Labels (1)
0 Kudos
Reply
1 Reply

1,945 Views
linestream-adam
Senior Contributor I

Mark,

We have not published the KMS UART command set. We didn't design the protocol to be made publicly available. It is a fairly simple protocol, but some of the advanced functionality (e.g. plotting) are difficult to configure and would be confusing to document. We don't have any plans to release the serial protocol.

0 Kudos
Reply