KMS GUI command set and syntax

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KMS GUI command set and syntax

2,112件の閲覧回数
M_Grillo
Contributor III

Hello, Is there a publicized KMS UART command set and syntax requirement/example document for the KV31? I’d like to multipurpose UART0 for the KMS-GUI, our own command set and possibly our own automated configuration setup/monitoring like the KMS GUI in a production piece of test equipment.

 

Thanks,

Mark

ラベル(1)
0 件の賞賛
返信
1 返信

1,926件の閲覧回数
linestream-adam
Senior Contributor I

Mark,

We have not published the KMS UART command set. We didn't design the protocol to be made publicly available. It is a fairly simple protocol, but some of the advanced functionality (e.g. plotting) are difficult to configure and would be confusing to document. We don't have any plans to release the serial protocol.

0 件の賞賛
返信