Auto lead angle algorithm on KV31 or KMS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Auto lead angle algorithm on KV31 or KMS

1,832 次查看
jackjamieson
NXP Employee
NXP Employee

Can KV31 parts or Kinetis Motor Suite do the algorithm mentioned in the below article?

https://www.semanticscholar.org/paper/Auto-lead-angle-algorithm-for-high-efficiency-of-Jeon-Park/734...

标签 (1)
0 项奖励
回复
1 回复

1,719 次查看
linestream-adam
Senior Contributor I

Since Kinetis Motor Suite implements Field Oriented Control, the angle is always placed for maximum efficiency. Only in the most high speed motor control cases do you need to advanced the field angle due to the lag of calculations in the main interrupt.

The paper you link to is designed for trapezoidal motor control which is typically less efficient than FOC and needs to use tricks like this in order to improve the efficiency.

0 项奖励
回复