where to get source code of FRDM-KL25Z_QSP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

where to get source code of FRDM-KL25Z_QSP

1,986 次查看
hotashu
Contributor III
  • FRDM-KL25Z_QSP: FRDM-KL25Z Quick start package includes a set of "Precompiled Examples", where can i get the source code of them?
0 项奖励
回复
4 回复数

1,488 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Holy,

After you download the FRDM-KL25Z_QSP.Zip file, then extract the file and you will find the sub-folder Precompiled Examples in the FRDM-KL25Z_QSP folder.

I also attach the FRDM-KL25Z_QSP.Zip and you can have a try.

0 项奖励
回复

1,488 次查看
hotashu
Contributor III

hi Zhou,

there are two folder (OpenSDA Applications) and ( Precompiled Examples ) inside the package. but none of them includes the source code(include .c and .project. etc). where are those?

0 项奖励
回复

1,488 次查看
Mario_Guardado
Senior Contributor I

Hi,

As Zhou commented, you can download sample code (including .c and .project) from the following link:

KL25_SC: FRDM-KL25Z and TWRKL25Z48M Sample Code Package.

It is an .exe file, first you need to extract the content. It contains two folders,

1) klxx-sc-baremetal.

     For baremetal projects including CW, IAR and Keil examples.Similar projects than "Precompiled Examples" on FRDM-KL25Z_QSP file can be found      here.

2) klxx-sc-pex.

     For Processor Expert examples.

I hope it helps.

0 项奖励
回复

1,488 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Holy,

I think you don't exactly know about OpenSDA interface mode,There's none of sourece code could be found in the Precompiled Examples is right.

If you want to look for demo code, you can through the link below to download.

FRDM-KL25Z Product Summary Page

0 项奖励
回复