where to get source code of FRDM-KL25Z_QSP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

where to get source code of FRDM-KL25Z_QSP

1,994 Views
hotashu
Contributor III
  • FRDM-KL25Z_QSP: FRDM-KL25Z Quick start package includes a set of "Precompiled Examples", where can i get the source code of them?
0 Kudos
Reply
4 Replies

1,496 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Holy,

After you download the FRDM-KL25Z_QSP.Zip file, then extract the file and you will find the sub-folder Precompiled Examples in the FRDM-KL25Z_QSP folder.

I also attach the FRDM-KL25Z_QSP.Zip and you can have a try.

0 Kudos
Reply

1,496 Views
hotashu
Contributor III

hi Zhou,

there are two folder (OpenSDA Applications) and ( Precompiled Examples ) inside the package. but none of them includes the source code(include .c and .project. etc). where are those?

0 Kudos
Reply

1,496 Views
Mario_Guardado
Senior Contributor I

Hi,

As Zhou commented, you can download sample code (including .c and .project) from the following link:

KL25_SC: FRDM-KL25Z and TWRKL25Z48M Sample Code Package.

It is an .exe file, first you need to extract the content. It contains two folders,

1) klxx-sc-baremetal.

     For baremetal projects including CW, IAR and Keil examples.Similar projects than "Precompiled Examples" on FRDM-KL25Z_QSP file can be found      here.

2) klxx-sc-pex.

     For Processor Expert examples.

I hope it helps.

0 Kudos
Reply

1,496 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Holy,

I think you don't exactly know about OpenSDA interface mode,There's none of sourece code could be found in the Precompiled Examples is right.

If you want to look for demo code, you can through the link below to download.

FRDM-KL25Z Product Summary Page

0 Kudos
Reply