where can i get the GPIO CAN code for k20d72m?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

where can i get the GPIO CAN code for k20d72m?

1,179件の閲覧回数
sreevenkedesh
Contributor I

hi 

  i am working on k20d72m, i need a  can code for   simple transmit and receive( need code which doesn't have OS dependency).

thanks in advance

タグ(3)
0 件の賞賛
返信
1 返信

1,115件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

There is an CAN example code (without OS) for TWR-K20D72M board located at CodeWarrior MCU V10.6 installation path:

C:\Freescale\CW MCU v10.6\MCU\CodeWarrior_Examples\Processor_Expert\Kinetis\TWR-K20D72M\CAN

Customer can download CodeWarrior MCU V10.6 software from below link:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MCU10&fpsp=1&tab=Design_Tools_Tab


Wish it helps.
best regards
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信