where are TWR-KW24512 docs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

where are TWR-KW24512 docs

ソリューションへジャンプ
1,600件の閲覧回数
JonathanHess
Contributor III

Got my tower system module with KW24 and have read the quick start guide but… where is the rest of the documentation?

Something that talks about what all the jumpers are and a schematic?

Where is the tower configuration spreadsheet for the module?

And… since I think I inadvertently wiped the program that was provided with it, where can I download the default program so I can reload it?

Very little appears to be on the OpenSDA partition on the device itself.

0 件の賞賛
返信
1 解決策
1,456件の閲覧回数
Wlodek_D_
Senior Contributor II

Hello Jonathan,

Please see answer (where are TWR-KW24D512 docs ) to your repeated question posted in another place and follow Paul's advice .

Thank you and regards,

Wlodek_D.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,457件の閲覧回数
Wlodek_D_
Senior Contributor II

Hello Jonathan,

Please see answer (where are TWR-KW24D512 docs ) to your repeated question posted in another place and follow Paul's advice .

Thank you and regards,

Wlodek_D.

0 件の賞賛
返信