watchdog timer not resetting even after timing out refresh count for MKL26Z256VLH4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

watchdog timer not resetting even after timing out refresh count for MKL26Z256VLH4

3,215件の閲覧回数
omkar_virkar
Contributor II

I am working on watchdog timer of MKL26Z256VLH4, I have flashed cop sample application and it worked perfectly fine. but when I included cop function in my current program, COP is refreshing but it is not resetting after the loopcount is finished.

/* Check if WDOG reset occurred */
if (RCM_GetPreviousResetSources(RCM) & kRCM_SourceWdog)
{
PRINTF("Reset due to COP timeout\r\n");
COP_Disable(SIM);
PRINTF("COP example ends!\r\n");
}
else
{
/* If WDOG reset is not occurred, enables COP */
PRINTF("\r\nCOP example start!\r\n");
COP_Init(SIM, &configCop);
/* Refresh COP 10 times and then wait for timeout reset */
for (uint32_t loopCount = 0U; loopCount < 10U; loopCount++)
{
COP_Refresh(SIM);
PRINTF("COP refresh %d time\r\n", loopCount + 1U);
}

PRINTF("COP will timeout and chip will be reset\r\n");
}

while (1)
{}

   

omkar
0 件の賞賛
返信
2 返答(返信)

3,206件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi omkar,

If you are using SDK example, then please notice the definition of DISABLE_WDOG.

DISABLE_WDOG.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

3,210件の閲覧回数
bobpaddock
Senior Contributor IV

Check the datasheet for timing limits on COP. 

Usually COP can only be disabled/enabled within so many cycles of a physical reset.

It may also be a write once thing, make sure that some bootloader is not disabling it.

Move the COP code as close to the start of main() as your hardware setup will allow.
Ideally COP would be first, however sometime I/O needs dealt with faster.

At a minimum move the COP instructions before the printf()s, those take a lot of cycles.