using the MK22FX512VLL12. Does the USB (device) require 5V into VREGIN to operate? A separate 3.3V source is applied to VDD.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

using the MK22FX512VLL12. Does the USB (device) require 5V into VREGIN to operate? A separate 3.3V source is applied to VDD.

1,103件の閲覧回数
brandontaylor
Contributor I

Does the internal transceiver only get power from VREGIN?

0 件の賞賛
返信
1 返信

972件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Brandon:

Yes the transceiver gets its power from the Vreg, so you must connect VREGIN. It does not have to be 5V. according to datasheet you can wire VREGIN to VDD (3.3V)

Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信