using the MK22FX512VLL12. Does the USB (device) require 5V into VREGIN to operate? A separate 3.3V source is applied to VDD.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

using the MK22FX512VLL12. Does the USB (device) require 5V into VREGIN to operate? A separate 3.3V source is applied to VDD.

1,098 Views
brandontaylor
Contributor I

Does the internal transceiver only get power from VREGIN?

0 Kudos
Reply
1 Reply

967 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Brandon:

Yes the transceiver gets its power from the Vreg, so you must connect VREGIN. It does not have to be 5V. according to datasheet you can wire VREGIN to VDD (3.3V)

Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply