using processor expert to create component codes

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

using processor expert to create component codes

1,477 次查看
omerbulut
Contributor III

I have a MKL26Z128VFT Freescale Microcontroller. I want to use additional crystal capacitor for USB communication, I mean it needs 48 MHz. I cannot create and add its library with the Processor Expert. Could you suggest me way that can works for it? thank you very much..

0 项奖励
回复
1 回复

1,331 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi  &Ouml,

      Could you tell me what the external crystal you are using? 8MHZ?

      If yes, you can configure the PE like the following picture, and choose your USB clock source to the MCGPLLCLK, then the USB clock will be 48Mhz.

37.jpg

38.jpg

Wish it helps you!

If you still have question, please contact with me!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------