using MATLAB/Simulink to Program Kinetis Microcontrollers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

using MATLAB/Simulink to Program Kinetis Microcontrollers

2,331件の閲覧回数
saeidsaeidi
Contributor I

Hi,

I am using embedded coder of Mathworks to develop code for Kinetis microcontrollers. I installed the Motor Control Toolbox of NXP. However the target microcontroller I am using (MKV11Z128) is not listed in MATLAB. Only MKV10xxx series are available to choose in MATLAB.

A further Problem is that after building the model including the Motor Control Toolbox blocks, no IAR project is created, and the source code needs to be integrated in an IAR Project manually. Is it the standard workflow?!

Best regards

Saeid

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,965件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

Regarding the second question for IAR, you need to create a new project by selecting the "Externally built executable option" that will no need to integrate source code manually.

0 件の賞賛
返信

1,965件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

When you install the Motor Control Toolbox, on the installation folder there is a document Motor_Control_Toolbox_Release_Notes with the list of supported device, unfortunately as you said the MKV11Z128VLF7 is not supported.

You can check the list and maybe you can use on your project the MKV31.

Regards

Vicente Gomez

0 件の賞賛
返信