We am having another doubt here,MrPedro
We are planning to use the KSZ8041NL Ethernet phy(The same , which is used in the TWR-SER)
This is the first time we are using Ethernet,so we have a few quires understanding the connections in the tower board:
We are planning to use in RMII mode.
1. If we provide an external reference clock of 50Mhz to the Ethernet PHY(pin 9), then there is no need to provide the XTAL signal from the K60 MCU also?
Currently we have disabled the 50Mhz oscillator in code warrior.and we keep getting this warning.Please refer to the image.Is it acceptable to ignore this warning there is already an external reference clock providing the signal to the Ethernet PHY IC?

2. As we are using RMII mode,there is no need fro RXD3,TXD3,RXD2,TXD2,(pin 13,14,26 and 27)so can we leave these pins in open connection or should we ground these pins?
Thanks in advance,
Arun