usb enumeration failed in usbFS in MK70

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

usb enumeration failed in usbFS in MK70

1,433 Views
dhanalakshmisre
Contributor I

usb enumeration failed in usbFS in MK70 and it shows usb error

Labels (1)
0 Kudos
Reply
1 Reply

1,359 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

NXP provides K70 bare metal sample code, which includes USB device/host demo project.

Customer could download the Kinetis 120MHz bare metal sample code from here.

NXP also provide USB Stack V5.0 for TWR-K70F120M board, please download USB Stack V5.0 from here.


Wish it helps
Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply