usb enumeration failed in usbFS in MK70

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

usb enumeration failed in usbFS in MK70

1,434件の閲覧回数
dhanalakshmisre
Contributor I

usb enumeration failed in usbFS in MK70 and it shows usb error

ラベル(1)
0 件の賞賛
返信
1 返信

1,360件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

NXP provides K70 bare metal sample code, which includes USB device/host demo project.

Customer could download the Kinetis 120MHz bare metal sample code from here.

NXP also provide USB Stack V5.0 for TWR-K70F120M board, please download USB Stack V5.0 from here.


Wish it helps
Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信