usb_cdc k20

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

usb_cdc k20

2,306件の閲覧回数
kooroshhajiani
Contributor III

Hi,

I have 2 boards, the targets are k64 and k20(MK20DN64XXX5) repectively.

Requirements calls for boards to communicate over USB , Just simple Data back and forth, This link would replace the UART link on the newer design. While I am not an expert in USB communication, I decided to use CDC class for this, I HOPE THIS IS THE RIGHT CHOICE!!!!.

To that end ,I was able to use one of the demos in KDS to build code for the K64  target board as a  USB CDS host, I have added Freertos to that and seems to be running  OK, however to be able to test the USB I need to have the k20 target running as USB CDC device but I can't find any support for this in KDS or in DSK demos and examples.

I tried to use processor expert in KDS for the K20 target but when I looked at the component list I don't see any FSL_USB for the CDC class.

Am I missing something here?

Is USB CDC class the right choice for simple request and response over usb link?

Where would I find support for the USB CDC for k20 target.

Please I need help.

Regards,

Koorosh Hajiani

タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,087件の閲覧回数
Jiun_Yong
Contributor III

Hi Koorosh

From my experience, USB CDC class is a suitable solution for transmitting data between your board and a host. If you connect the USB port to a Windows PC, it should come up in Device Manager as a COM port.

If you want to learn more about USB protocol, I recommend the book "USB Complete" by Jan Axelson. See this link: Jan Axelson's Lakeview Research

Good luck

Steve

0 件の賞賛
返信

2,087件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Koorosh Hajiani:

The latest NXP USB stack supporting the Kinetis K20_50MHz family was the USB Stack V4.1.1. It is available from the next link but unfortunately this is a legacy package and does not include projects for KDS, only for CodeWarrior, IAR and Keil:

USB Stack|NXP

A good alternative would be to use the USB components provided by colleague Erich Styger. See this article for the K20:

USB CDC with the FRDM-K20D50M | MCU on Eclipse

The related Processor Expert components from that tutorial are not delivered by default with KDS, those have to be installed:

McuOnEclipse Releases on SourceForge | MCU on Eclipse

Regards!

Jorge Gonzalez

2,087件の閲覧回数
kooroshhajiani
Contributor III

Hi Jorge,

Many thanks for your reply.

So I have the USB_HOST_CDC demo running on the TWR64F12+ser2 board, I downloaded the  USB Stack V4.0.3 and was able to build the CDC_DEVICE for k20 target using IAR WORK BENCH evaluation compiler.

Then I downloaded it to the K20 target using KDS ide and PE MULTILINK box. I plugged the device (K20) in the PC and I can see that the PC tries to download the drivers which of course it fails.

HOWEVER WHEN I plugged the k20(device) in the K64+SER2 USB socket nothing happened . The host code running on the 64k+Ser2 board does not even try to attach. I am not an expert in USB and this is the first time I'm trying to do USB.

I checked all the relevant jumpers on the TWR_K64 and SER2 board and they seem to be correct. the HOST software running on K64 target is the USB_HOST_CDC_SERIAL demo in the SDK

.Pleas, any help is truly appreciated.

Thanks,

Koorosh Hajiani

0 件の賞賛
返信