uTasker for Kinetis Update (PPP, FT800, FreeRTOS, MCUXpresso)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

uTasker for Kinetis Update (PPP, FT800, FreeRTOS, MCUXpresso)

1,666件の閲覧回数
mjbcswitzerland
Specialist V

Hi All

Here is a link to new uTasker features that may be of interest to professionals who are looking for ways of improving Kinetis development efficiency and reducing development times:
http://www.utasker.com/forum/index.php?topic=1947.0

Fans of FreeRTOS may be especially interested in the fact that FreeRTOSv9.0.0 can be natively integrated (no port required) to achieve a dual-operating system design. This allows FreeRTOS users to immediately benefit from new integrated libraries (such as wide-feature TCP/IP, FAT, USB and MODBUS) along with the capability to reduce code size / RAM requirements in Kinetis based projects.


It is hoped that full (approx. real-time) Kinetis simulation (peripherals, interrupts, DMA) will also soon be available to the pre-emptive FreeRTOS part as well as the uTasker part which has the potential to open a new dimension in Visual Studio based accelerated developments in such designs too!


Just request in case of interest in demonstrations (on any Kinetis part).

Regards

Mark

http://www.utasker.com/kinetis.html

タグ(2)
0 件の賞賛
返信
1 返信

1,402件の閲覧回数
mjbcswitzerland
Specialist V

Hi All

Here is a short video showing a simulated FRDM-K64F and FTDI's FT800 emulator integrated together running slightly modified FTDI reference code (to allow non-blocking operation):
https://www.youtube.com/watch?v=XxC3Y2NaaU8

Regards

Mark

0 件の賞賛
返信