tool to program and debug a custom board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

tool to program and debug a custom board

ソリューションへジャンプ
3,413件の閲覧回数
peralesserrano
Contributor I

hi i want tool to program and debug a custom board with KDS, i want use kinetis K70 in custom board, and I would like that could also be used to to debug i.mx6 for the future.

I look for a tool like PIC ICD3 for example, but for Kinetis

thanks

PD: sorry for my english

0 件の賞賛
返信
1 解決策
3,235件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

In general, we recommend customer to use P&E USB Multilink Universal tool or Segger  J-Link tool.

And for the cost consideration, it also could use Kinetis FROM board embedded OpenSDA debugger tool, such as FRDM-KL05Z.

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,236件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

In general, we recommend customer to use P&E USB Multilink Universal tool or Segger  J-Link tool.

And for the cost consideration, it also could use Kinetis FROM board embedded OpenSDA debugger tool, such as FRDM-KL05Z.

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,235件の閲覧回数
peralesserrano
Contributor I

thank you very much,

the Segger says that does not implement SWO for KDS IDE, this is important?

0 件の賞賛
返信
3,235件の閲覧回数
dave408
Senior Contributor II

SWO enables things like printf and variable watching, but I don't think it's the only way to get those features.  I am able to set watches just fine in my code without SWO, and if I really need printf, I enable semihosting and my console output appears in a dedicated window in KDS, which is nice.

0 件の賞賛
返信