the difference between MK20DN512VMD10 and MK20DN512ZVM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

the difference between MK20DN512VMD10 and MK20DN512ZVM

1,169 Views
davidsui
Contributor I

I am using MK20DN512ZVM and the sales told me MK20DN512VMD10 is a newer version and send me some samples. then I replace it on my board, but I found the MQX doesn't run! then I analyzed this problem and found out that MCU(MK20DN512VMD10) will reset when run this function.

void PE_low_level_init(void)

{

      /* Initialization of the SIM module */

  /* SIM_SOPT6: RSTFLTEN=0,RSTFLTSEL=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0 */

  SIM_SOPT6 = (uint32_t)0x00UL;        /* Set reset pin filter */

      /* Initialization of the PMC module */

  /* PMC_LVDSC1: LVDACK=1,LVDIE=0,LVDRE=1,LVDV=0 */

  PMC_LVDSC1 = (uint8_t)((PMC_LVDSC1 & (uint8_t)~(uint8_t)0x23U) | (uint8_t)0x50U);

  /* PMC_LVDSC2: LVWACK=1,LVWIE=0,LVWV=0 */

  PMC_LVDSC2 = (uint8_t)((PMC_LVDSC2 & (uint8_t)~(uint8_t)0x23U) | (uint8_t)0x40U);

  /* PMC_REGSC: TRAMPO=0,??=0,BGBE=0 */

  PMC_REGSC &= (uint8_t)~(uint8_t)0x13U;

  /* SIM_SCGC4: LLWU=1 */

  SIM_SCGC4 |= (uint32_t)0x10000000UL;

        /* Initialization of the LLWU module */

  /* LLWU_PE1: WUPE3=0,WUPE2=0,WUPE1=0,WUPE0=0 */

  LLWU_PE1 = (uint8_t)0x00U;

  /* LLWU_PE2: WUPE7=0,WUPE6=0,WUPE5=0,WUPE4=0 */

  LLWU_PE2 = (uint8_t)0x00U;

  /* LLWU_PE3: WUPE11=0,WUPE10=0,WUPE9=0,WUPE8=0 */

  LLWU_PE3 = (uint8_t)0x00U;

  /* LLWU_PE4: WUPE15=0,WUPE14=0,WUPE13=0,WUPE12=0 */

  LLWU_PE4 = (uint8_t)0x00U;

  /* LLWU_ME: WUME7=0,WUME5=1,WUME4=0,WUME3=0,WUME2=0,WUME1=0,WUME0=0 */

  LLWU_ME = (uint8_t)((LLWU_ME & (uint8_t)~(uint8_t)0x9FU) | (uint8_t)0x20U);

  /* LLWU_CS: ACKISO=1,??=1,FLTEP=0,FLTR=0 */

  LLWU_CS = (uint8_t)((LLWU_CS & (uint8_t)~(uint8_t)0x03U) | (uint8_t)0x84U);

}

then I checked the newest ref manual. it confused me much!

pastedImage_1.png

is there anyone could help to explain that?

0 Kudos
Reply
1 Reply

1,088 Views
santiago_gonzal
NXP Employee
NXP Employee

Hello,

You can check this AN to get the full information of the changes between the two silicon versions:

http://cache.freescale.com/files/32bit/doc/app_note/AN4445.pdf

Regards,

Santiago

0 Kudos
Reply