I'm using FRDM-KE06Z board and CW 10.6.4. I have configured 6 PWM outputs through FTM2 period device which has 6 available channels. Everything is working ok and I have uploaded the program to the board but I need to get access to the PTG5, PTG6 and PTG7 pin out signals and I can't find them. I know this outputs are used by the RGB led but they don't appear at the pinout description. I must get at least PTG6 output signal because the PWM configuration don't allow me to avoid this pins.
Thanks in advance !
Kind Regards.
![pastedImage_1.png pastedImage_1.png](/t5/image/serverpage/image-id/36221i3B751CDEE5FAE74F/image-size/large?v=v2&px=999)