tera term tutorial

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

tera term tutorial

3,789 Views
josephg
Contributor II

While watching the a video on setting up the Freedom Development Board, I was directed to go to the tera term tutorial.  Once tera term was installed and the serial port set up I was to see data flowing.  I did not see data flowing.  I was able to press the reset button on the development board and see a menu from the development board.  I selected a few of the menu options and nothing happened.

Below is the link to the video

https://f1.media.brightcove.com/12/4089003392001/4089003392001_5086059391001_4504345637001.mp4?pubId...

I am also including a screen shot of the menu sent to the computer from the development board.

tera term menu.png

I contacted the chat line and was told to post it here.

Has anyone else had such problems and if so is there a solution or is this something I should just ignore for now and just try the IDE?

Labels (1)
0 Kudos
Reply
1 Reply

3,588 Views
mjbcswitzerland
Specialist V

Hi Joseph

It looks to be working but I think the pre-installed demos interact much on the UART.

Try some more demos for your board from here, which allows more interaction: http://www.utasker.com/kinetis.html

You may also find a video for your board at
https://www.youtube.com/watch?v=kWNlsAoMly4&list=PLWKlVb_MqDQFZAulrUywU30v869JBYi9Q


Regards

Mark

0 Kudos
Reply