stdbool.h header with the GNU/ARM C for Kinetis L

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

stdbool.h header with the GNU/ARM C for Kinetis L

2,335 Views
steve_fae
Senior Contributor I

can stdbool.h header be used with the GNU/ARM C?

0 Kudos
Reply
5 Replies

1,903 Views
JimDon
Senior Contributor III

That's really not the best answer. I think what should happen is that you should use lib_c99.prefix instead of lib_ewl.prefix but  right now I don't know how do that, nor am I 100% sure of other side effects.

I just discovered http://cache.freescale.com/files/soft_dev_tools/doc/ref_manual/EWL_C_Reference.pdf but right now I don't have time to read it....see page 163

of this document.

"The facilities in this header file are only available when the compiler is configured to

compile source code for C99 (ISO/IEC 9899:1999). Refer to the Build Tools Reference for

information on compiling C99 source code." (ed. Really? Why?)

My thoughts:

(a slow sigh*) I don't see the big deal over defining bool, true and false. For some reason, the "C" gods have  made a deal out of this. If this is really the only issue, then you could advise that the user just do this - define bool true and false.

* to let out one's breath audibly, as from sorrow, weariness, or relief.

0 Kudos
Reply

1,903 Views
JimDon
Senior Contributor III

Yes.

0 Kudos
Reply

1,903 Views
steve_fae
Senior Contributor I

Ah, I didn't add, customer asked because they get this warning.

_EWL_C99 macro is not defined

0 Kudos
Reply

1,902 Views
JimDon
Senior Contributor III

Add this at the top of the file:

#undef _EWL_C99

#define _EWL_C99 1

The warning will be gone.

1,903 Views
JimDon
Senior Contributor III

Or put it in derivative.h