sleep mode download

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

sleep mode download

1,198件の閲覧回数
geniusgogo
Contributor I

i used MKL15z chip,entry LLS mode after power up.

because not wakeup,so can't download,

What should I do?

0 件の賞賛
返信
1 返信

1,127件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

If you have Segger J-Link Commander, try to connect KL15 during reset. For example:

1. Power Off the board

2. Press the Reset Button

3. Power ON the board

4. Connect the MCU using J-Link Commander (Mass erase the MCU)

6. Release the Reset Button

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信