silicon revision for K20 family

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

silicon revision for K20 family

924件の閲覧回数
ivanxie
Contributor I

I want to know the difference of each silicon revision, such as Initial, Main and Revision after main.

For example, how to swap using between MK20DN512VLK10 vs MK20DN512ZVLK10?

Thanks.

0 件の賞賛
返信
1 返信

916件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

There are a lot of difference between MK20DN512ZVLK10(Rev1.x) and MK20DN512ZVLK10(Rev2.x). Customer should notice Hardware and Software impact descripted in AN4445.

Rev1.x is not in the support list of KSDK and MCUXpresso SDK .
So I am afraid you may need to develop it by using the Processor Expert in KDS3.2 or CW11.

If you have never used Processor Expert, then please refer:
Overview: Processor Expert
Getting Help on Processor Expert Components

There are several examples of typical settings and usage of xxx_LDD component. You can modify the setting in processor expert and copy the codes.

_LDD Typical Usage.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信